MC_Stop
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Execute |
BOOL |
0, 1 |
N/A |
No default |
On the rising edge The transition of a digital signal from low to high. AKA: positive edge., request to stop the axis. It can be held high to prevent any other moves from being queued. |
Axis |
AXIS_REF |
1, 256 |
N/A |
No default |
Name of a declared instance of the AXIS_REF library function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances..
|
Deceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Trapezoidal: Deceleration rate. S-curve: Unused. |
LREAL |
No range |
User unit/sec3 |
No default |
Trapezoidal: 0 (zero). S-curve: Constant jerk. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Done |
BOOL |
|
|
Indicates both:
|
Busy |
BOOL |
|
|
High from the time both:
|
Active |
BOOL |
|
|
High from the time both:
|
Error |
BOOL |
|
|
Indicates an invalid input was specified. |
ErrorID |
INT |
|
|
Indicates the error if the Error output is set to TRUE. |
Remarks
-
- This function block starts a motion-related action and stores data for calculations and error checking.
See Call Function Blocks Multiple Times in the Same Cycle if using a dual-core controller.
- See Function Blocks - General Rules about how inputs and outputs work.
- An MC_Stop cannot be aborted.
- This means that, while in Stopping state, no function block can command any motion on the axis.
- The axis remains in Stopping state until it reaches zero velocity and the Execute input is low.
- The application program The act of performing a sequence of instructions or commands. can hold the axis in Stopping state even after it reaches zero velocity by leaving the Execute input high.
- It aborts any ongoing function block execution.
- When the Done output is set, the state transfers to StandStill.
- While the axis is in Stopping state, no other FB can perform any motion on the same axis.
Figure 1: MC_Stop
Time Diagram
This example shows the behavior of the combination of a MC_Stop FB with a MC_MoveVelocity.
- A rotating axis is ramped The gradual acceleration and deceleration of a stepping motor. This is essential if performance beyond the start/stop range is required. The slope of the ramp is a function of screw pitch, load, drive voltage and design, and motor. down with FB2 MC_Stop
- The axis rejects motion commands as long as MC_Stop parameter “Execute” = TRUE
FB1 MC_MoveVelocity reports an error indicating the busy MC_Stop command.
Figure 2: Time Diagrams: First and Second FBs
Figure 3: Time Diagram
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MC_Stop S T example *) Inst_MC_Stop( StopRequest , Axis1, 100.0, 100.0 ); //Inst_MC_Stop is an instance of MC_Stop function block StopComplete := Inst_MC_Stop.Done; //store the Done output into a user defined variable StopActive := Inst_MC_Stop.Active; //store the Active output into a user defined variable StopError := Inst_MC_Stop.Error; //store the Error output into a user defined variable