MC_ReadActVel
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BOOL |
FALSE, TRUE |
N/A |
No default |
Request to read the axis's actual velocity. |
|
Axis |
AXIS_REF |
1, 256 |
N/A |
No default |
Name of a declared instance of the AXIS_REF library function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances..
|
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Valid |
BOOL |
FALSE, TRUE |
N/A |
Indicates the value at the ActualVelocity output is available. |
Busy |
BOOL |
FALSE, TRUE |
N/A |
Indicates this function block is executing. |
Error |
BOOL |
FALSE, TRUE |
N/A |
Indicates an invalid input was specified. |
ErrorID |
INT |
-32768 to +32767 |
|
Indicates the error if Error output is TRUE. |
ActualVelocity |
LREAL |
|
User unit/sec |
Oscillations may be seen because this is an instant velocity, not an average velocity. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
See Function Blocks - General Rules about how inputs and outputs work.
Figure 1: MC_ReadActVel
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
* MC_ReadActVel S T example *); Inst_MC_ReadActVel( TRUE, Axis1 ); //Inst_MC_ReadActVel is an instance of MC_ReadActVel function block ActualVel := Inst_MC_ReadActVel.ActualVelocity; // store ActualVelocity output into a user defined variable