MC_MoveAdditive
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Execute |
BOOL |
0, 1
|
N/A |
No default |
On the rising edge The transition of a digital signal from low to high. AKA: positive edge., request to queue the move. |
Axis |
AXIS_REF |
1, 256 |
N/A |
No default |
Name of a declared instance of the AXIS_REF library function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances..
|
Distance |
REAL |
No range |
User units |
No default |
Distance to add to the endpoint of the previous move. |
LREAL |
No range |
User unit/sec |
No default |
Velocity setpoint The target value that an automatic control system (e.g., PID controller) aims to reach.. |
|
LREAL |
No range |
User unit/sec2 |
No default |
Trapezoidal: Acceleration rate. S-curve: Maximum acceleration. |
|
Deceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Trapezoidal: Deceleration rate. S-curve: Unused. |
LREAL |
No range |
User unit/sec3 |
No default |
Trapezoidal: 0 (zero). S-curve: Constant jerk. |
|
BufferMode |
SINT |
0, 5 |
N/A |
No default |
|
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Done |
BOOL |
No range
|
N/A |
Indicates the move completed successfully. |
Busy |
BOOL |
No range
|
N/A |
High from the moment the Execute input goes high until the time the move is ended. |
Active |
BOOL |
No range
|
N/A |
Indicates this move is the Active move. |
CommandAborted |
BOOL |
No range
|
N/A |
Indicates the move was aborted. |
Error |
BOOL |
No range
|
N/A |
Indicates either:
|
ErrorID |
INT |
No range
|
N/A |
Indicates the error if Error output is TRUE. |
Remarks
-
- This function block starts a motion-related action and stores data for calculations and error checking.
See Call Function Blocks Multiple Times in the Same Cycle if using a dual-core controller.
- See Function Blocks - General Rules about how inputs and outputs work.
- It is typically used with Abort specified at the BufferMode input.
- If BufferMode is not Abort, this move is identical to an MC_MoveRelative.
Figure 1: MC_MoveAdditive
Time Diagram
These images show two examples of the combination of two Function Blocks (FBs) while the axis is in Discrete Motion state:
- The left part of the diagram illustrates when the second FB is called after the first one.
- If the first reaches the commanded distance 6000, and the velocity is 0 (zero), the output Done causes the second FB to move to the distance 10000.
- The right part of the diagram illustrates when the second move FB starts the execution while the first FB is still executing.
- The first motion is interrupted An asynchronous signal from hardware indicating the need for attention or a synchronous event in software indicating the need for a change in execution. and aborted by the Test signal during the constant velocity of the first FB.
- The second FB:
- Adds on the previous commanded position of 6000 the distance 4000.
- Moves the axis to the resulting position of 10000.
Figure 2: Time Diagrams: First and Second FBs
Figure 3: Time Diagram
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MC_MoveAdditive ST example *)
Inst_MC_MoveAdditive( MovAddReq, Axis1, 123.456, 100.0, 100.0, 100.0, 0, 0 ); //Inst_MC_MoveAdditive is an instance of MC_MoveAdditive function block
MovAddDone := Inst_MC_MoveAdditive.Done; //store Done output into user defined variable
See Also