MLAxisAddTq
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Set the additive torque The tendency of a force to rotate an object about an axis. A force is a push or a pull; a torque is a twist. value to the drive In electrical engineering, a drive is an electronic device to provide power to a motor or servo. Control device for regulating the speed, torque and position of a motor. A unit controlling a motor using the current and timing in its coils. output (torque feed-forward This describes an element or pathway within a control system which passes a controlling signal from a source in the control system's external environment, often a command signal from an external operator, to a load elsewhere in its external environment.).
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
ID |
DINT |
No range |
N/A |
No default |
Pipe network identifier of the axis block. |
Torque |
LREAL |
No range |
Rated torque units as used in the drive. Example: Rated motor An actuator focused to a movement, converting electrical energy in a force or torque. continuous torque X the Torque factor. |
No default |
Requested additive torque value in N.m (Newton meter). |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. |
Remarks
-
-
This function or function block A function block groups an algorithm and a set of private data. It has inputs and outputs. returns cached data.
See Program a Multi-Core Controller.
- This function is only active after the MLAxisRatedTq function has been invoked.
- Using the PDOs for AKD, AKD2G, AKD-N, S300, or S700, it also requires the IL.KBUSFF value to be set to 1 in the drive.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisAddTq(PipeNetwork.Axis1, LREAL#10 ) ;
See Also