MLAxisGenWriteSpd
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sets the speed Speed is the absolute value of the velocity without direction. of the internal generator of an axis.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
AxisID |
DINT |
No range |
N/A |
No default |
ID Name of the Axis block. |
Speed |
LREAL |
No range |
User units |
No default |
Sets the generator Speed value. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. |
Remarks
This function or function block A function block groups an algorithm and a set of private data. It has inputs and outputs. does not generate any motion.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisGenWriteSpd(PipeNetwork.Axis1, 500 ) ;
See Also