Gear
Name |
Description |
Initializes a Gear Pipe Block with user-defined settings and for use in a PLC Programmable Logic Controller - A digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events. program The act of performing a sequence of instructions or commands.. |
|
Returns the Offset value of a selected Gear Block from the Pipe Network. |
|
Returns the Offset Slope value of a selected Gear Block from the Pipe Network. |
|
Returns the Ratio value of a selected Gear Block from the Pipe Network. |
|
Returns the Ratio Slope value of a selected Gear Block from the Pipe Network. |
|
Sets the Offset value of a selected Gear Pipe Block. |
|
Sets the Offset Slope value of a selected Gear Pipe Block. |
|
Sets the Ratio value of a selected Gear Pipe Block. |
|
Sets the Ratio Slope value of a selected Gear Pipe Block. |
Examples of Gear Functions
The output value starts with offset = 0 and gain = 1 (blue line)
Call the MLGearWriteOff function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. to modify the Offset.
This is where Offset_Slope is set with the MLGearWriteOSlp function.
After setting the Offset (Q=TRUE in the previous figure), call the MLGearWriteRatio function to modify the gear Ratio.
This is where Gain_Slope is set with the MLGearWriteRatSlp function.
The output value is adapted with the gear offset and ratio (blue line).