AOUT#.SOURCE

Description

This keyword sets the source of the analog output

Value Description
0 AOUT#.VALUE is driven by AOUT#.VALUEU.
1 AOUT#.VALUE is driven by an action in the Action table
2 AOUT#.VALUE is driven by the associated fieldbus object
3 AOUT#.VALUE is driven by an event in the Sequencer

Examples

Usage

When AOUT#.SOURCE = 0 (User), then AOUT #.VALUE will be controlled by AOUT #.VALUEU.

When AOUT#.SOURCE = 1 (Action table), then AOUT #.VALUE will be controlled by the assigned action, if any.

When AOUT#.SOURCE = 2 (Fieldbus), then AOUT#.VALUE will be controlled by the associated fieldbus analog output object 3800h sub 2.

When AOUT#.SOURCE = 3 (Sequencer), then AOUT#.VALUE will be controlled by the assigned event in the Sequencer.

Code

Changing output value with VALUEU and then changing SOURCE to be action table with no action configured:

--> AOUT1.SOURCE
0 (User)
--> AOUT1.VALUE
0.000 V
--> AOUT1.VALUEU 1
--> AOUT1.VALUE
1.000 V
--> AOUT1.SOURCE 1
--> AOUT1.VALUE
0.000 V

Context

For more information see Analog Output.

Versions

Action Version Notes
Implemented 02-00-00-000  
Added fieldbus source 02-00-01-000  
Added Sequencer source 02-02-03-000  

General Information

Type Read/Write
Units N/A
Range 0 to 2
Default Value 0
Data Type Integer
See Also  
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AOUT1.SOURCE

3800h

03h

Unsigned8

-

-

Read/Write

No

AOUT2.SOURCE

3801h

03h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

24050

1

24050 (0x5df2)

AOUT1.SOURCE

Unsigned8

Read/Write

Yes

24051

1

24051 (0x5df3)

AOUT2.SOURCE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AOUT1.SOURCE

24050

Unsigned8

Read/Write

-

AOUT2.SOURCE

24051

Unsigned8

Read/Write

-