AOUT#.VALUEU

Description

Gets or sets the user command value of the specified analog output when AOUT#.SOURCE = 0 (user).

Examples

Usage

When AOUT#.SOURCE = 0 (user) then the corresponding AOUT#.VALUEU is used to drive the AOUT#.VALUE .

Code

Changing output value with VALUEU and then changing SOURCE to be action table with no action configured:

--> AOUT1.SOURCE 0 //user
--> AOUT1.VALUEU
0.000 V
--> AOUT1.VALUE
0.000 V
--> AOUT1.VALUEU 1
--> AOUT1.VALUE
1.000 V

Context

For more information see Analog Output.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units V
Range 0 to 10
Default Value 5
Data Type Float
See Also  
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AOUT1.VALUEU

3800h

06h

Signed16

-

1000:1

Read/Write

Yes

AOUT2.VALUEU

3801h

06h

Signed16

-

1000:1

Read/Write

Yes