AXIS#.IL.CMDMODE

Description

AXIS#.IL.CMDMODE selects the type of current command that is used in Torque mode.

Value Description
0 DQ current command: AXIS#.IL.CMDU sets the torque producing current that creates axis motion.
1 UVW current commands: AXIS#.IL.IUCMDU and AXIS#.IL.IVCMDU set the U and V phase currents, and the W phase current is calculated from them so that the sum of the three phase currents is zero. The axis locks at the position corresponding to the generated force.

The default AXIS#.IL.CMDMODE = 0 is appropriate in most situations, where the goal is to create rotary or linear motion without velocity or position control, simply using the drive’s ability to produce torque and commutate.

Occasionally during commissioning and in special applications, it is helpful to command phase currents directly using AXIS#.IL.CMDMODE = 1. For example, the UVW motor connections can be checked by comparing phase current commands to the corresponding feedbacks.

This command is in use only when AXIS#.OPMODE = 0 (Torque).

Versions

Action Version Notes
Implemented 02-07-03-000  

General Information

Type Read/Write
Units N/A
Range 0, 1
Default Value 0
Data Type Integer
See Also AXIS#.IL.CMDU , AXIS#.IL.IUCMDU, AXIS#.IL.IVCMDU
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5830

1

5830 (0x16c6)

AXIS1.IL.CMDMODE

Unsigned8

Read/Write

Yes

71366

2

5830 (0x16c6)

AXIS2.IL.CMDMODE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.CMDMODE

5830

Unsigned8

Read/Write

-

Related Topics

Current Loop