AXIS#.IL.IUCMDU

Description

AXIS#.IL.IUCMDU sets the phase U command when AXIS#.OPMODE = 0 (Torque mode) and AXIS#.IL.CMDMODE = 1 (Phase Current mode). It takes effect when AXIS#.IL.SETCMD runs, to ensure coherency with the phase V current command.

The sum of the phase U and V current commands determines the phase W current command:

Phase W current command = -(Phase U current command + Phase V current command)

AXIS#.IL.IUCMDU is subject to the current loop and motor protection limits. The actual phase U current command is given by AXIS#.IL.IUCMD.

AXIS#.IL.IUCMDU is set to zero if any of these conditions are met:

Example

The following commands set the phase U current command to 1.0 Arms and the phase V current command to -1.5 Arms. The phase W current command is set to 0.5 Arms internally.


--> AXIS1.OPMODE 0
--> AXIS1.IL.CMDMODE 1
--> AXIS1.EN
--> AXIS1.IL.IUCMDU 1.0
--> AXIS1.IL.IVCMDU -1.5
--> AXIS1.IL.SETCMD
--> AXIS1.IL.IUCMD
1.000 [Arms]
--> AXIS1.IL.IVCMD
-1.500 [Arms]
--> AXIS1.IL.IWCMD
0.500 [Arms]

Versions

Action Version Notes
Implemented 02-07-03-000  

General Information

Type Read/Write
Units Arms
Range Limits are applied to overall current magnitude. Lower limit: max(-AXIS#.MOTOR.IPEAK, AXIS#.IL.LIMITN) Upper limit: min(AXIS#.MOTOR.IPEAK, AXIS#.IL.LIMITP)
Default Value 0 Arms
Data Type Float
See Also AXIS#.IL.CMDMODE, AXIS#.IL.IUCMD, AXIS#.IL.IUCMDU, AXIS#.IL.SETCMD
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5831

1

5831 (0x16c7)

AXIS1.IL.IUCMDU

Signed32

Read/Write

Yes

71367

2

5831 (0x16c7)

AXIS2.IL.IUCMDU

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.IUCMDU

5831

Float

Read/Write

-

Related Topics

Current Loop