CANOPEN.SDOLOGDUMP
Description
Outputs the current SDO log. Logging is enabled and disabled using CANOPEN.SDOLOGEN. The log will record up to 100 SDO messages received by the drive. How logging is handled once capacity is reached can be changed with CANOPEN.SDOLOGMODE. The logged data returned is formatted for easier reading. It will show whether the SDO was a read or write request along with the data read or written. If an error is encountered with a request and an SDO Abort was sent, it will log the abort code and an error string.
| Value | Description |
|---|---|
| 0 | Disabled |
| 1 | Enabled (default) |
Examples
To stop logging once full:
-->CANOPEN.SDOLOGDUMP 139d:10h:06m:44s: Write (0x2f) (1a00h:00h) "TxPDO mapping parameter 1" Data: 0x00 0x00 0x00 0x00 139d:10h:06m:44s: Write (0x23) (1a00h:01h) "Mapping entry 1" Data: 0x10 0x00 0x41 0x60 139d:10h:06m:44s: Write (0x23) (1a00h:02h) "Mapping entry 2" Data: 0x20 0x00 0x64 0x60 139d:10h:06m:44s: Write (0x23) (1a00h:03h) "Mapping entry 3" Data: 0x20 0x00 0xf4 0x60 139d:10h:06m:44s: Write (0x2f) (1a00h:00h) "TxPDO mapping parameter 1" Data: 0x03 0x00 0x00 0x00 -->
Context
For more information, see SDO Logging.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-09-01-000 |
General Information
| Type | Info Command |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | String |
| See Also | CANOPEN.SDOLOGEN
CANOPEN.SDOLOGMODE |
| Stored in Non-Volatile Memory | No |