CANOPEN.SDOLOGMODE

Description

Changes how SDO logs are handled once the maximum capacity of 100 entries is reached. By default, old messages are discarded as new messages are received. This can be changed to stop logging and ignore new messages once the maximum capacity is reached.

Value Description
0 Rollover
1 Stop On Fill

Examples

To stop logging once full:

-->CANOPEN.SDOLOGMODE 1

Context

For more information, see SDO Logging.

Versions

Action Version Notes
Implemented 02-09-01-000

General Information

Type Read/Write
Units N/A
Range 0 – Discard old logs as new ones come in
1 – Ignore new logs once capacity is reached
Default Value 0 – Discard old logs as new ones come in
Data Type Integer
See Also CANOPEN.SDOLOGDUMP
CANOPEN.SDOLOGEN
Stored in Non-Volatile Memory Yes

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CANOPEN.SDOLOGMODE

300bh

07h

Unsigned8

-

-

Read/Write

No