CANOPEN.SDOLOGEN

Description

Enables (default) or disables the SDO logging capability on EtherCAT and CAN drives. When enabled, SDO messages are logged by the drive and can be viewed with CANOPEN.SDOLOGDUMP.

The SDO log is cleared every time the log is enabled, i.e., CANOPEN.SDOLOGEN changes from 0 to 1.

The message log can contain a maximum of one hundred entries. How the entries are handled once the limit is reached is determined by CANOPEN.SDOLOGMODE.

Value Description
0 Disabled
1 Enabled (default)

Examples

To enable the SDO log set CANOPEN.SDOLOGEN to 1.

-->CANOPEN.SDOLOGEN 1

Context

For more information, see SDO Logging.

Versions

Action Version Notes
Implemented 02-09-01-000

General Information

Type Read/Write
Units N/A
Range 0 - Disabled
1 - Enabled
Default Value 0 - Disabled
Data Type Integer
See Also CANOPEN.SDOLOGDUMP
CANOPEN.SDOLOGMODE
Stored in Non-Volatile Memory Yes

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CANOPEN.SDOLOGEN

300bh

06h

Unsigned8

-

-

Read/Write

No