AXIS#.SAFEPARAM.SSR_#.FUNCTIONACTIVATION

Description

Indicates whether the Safe Speed Range (SSR) safety function can be activated. The parameter allows one of the following values:

Value Description

0

Never active

1

Ready for activation

This function can only be used when a safe encoder is configured in the safety parameters.

 

Context

For complete SSR information refer to SSR (Safe Speed Range).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Never active)

Data Type

Integer

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SSR_1.FUNCTIONACTIVATION

3161h

01h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_2.FUNCTIONACTIVATION

3162h

01h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_3.FUNCTIONACTIVATION

3163h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_1.FUNCTIONACTIVATION

3261h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_2.FUNCTIONACTIVATION

3262h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_3.FUNCTIONACTIVATION

3263h

01h

Unsigned8

-

-

Read/Write

No