AXIS#.SAFEPARAM.SSR_#.TIMEFORVELINLIMITS
Description
Indicates the time for the velocity in limits for the Safe Speed Range (SSR) safety function. After this time, the monitoring can be activated if the velocity is already in the limits.
This value is t_L_SSR in the following diagram:
Context
For complete SSR information refer to SSR (Safe Speed Range).
Related safety parameters:
- AXIS#.SAFE.SSR_#.INTERNALSTATE
- AXIS#.SAFEPARAM.SSR_#.DECLIMIT
- AXIS#.SAFEPARAM.SSR_#.DECMONITOREN
- AXIS#.SAFEPARAM.SSR_#.FAULTREACTION
- AXIS#.SAFEPARAM.SSR_#.FSOE
- AXIS#.SAFEPARAM.SSR_#.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SSR_#.SAFEINPUT
- AXIS#.SAFEPARAM.SSR_#.TIMEDELAYDECMONITORING
- AXIS#.SAFEPARAM.SSR_#.TIMETOVELMONITORING
- AXIS#.SAFEPARAM.SSR_#.VELLOWERLIMIT
- AXIS#.SAFEPARAM.SSR_#.VELUPPERLIMIT
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
2-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
|
Type |
Read/Write |
|
Units |
Milliseconds |
|
Range |
[1, 60000] |
|
Default Value |
1 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.SAFEPARAM.SSR_1.TIMEFORVELINLIMITS |
3161h |
08h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
AXIS1.SAFEPARAM.SSR_2.TIMEFORVELINLIMITS |
3162h |
08h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
AXIS1.SAFEPARAM.SSR_3.TIMEFORVELINLIMITS |
3163h |
08h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
AXIS2.SAFEPARAM.SSR_1.TIMEFORVELINLIMITS |
3261h |
08h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
AXIS2.SAFEPARAM.SSR_2.TIMEFORVELINLIMITS |
3262h |
08h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
AXIS2.SAFEPARAM.SSR_3.TIMEFORVELINLIMITS |
3263h |
08h |
Unsigned16 |
- |
- |
Read/Write |
No |