EGEAR.PULSESOUT

Description

EGEAR.PULSESOUT is the number of position counts the motor moves for each EGEAR.PULSESIN number of encoder counts. EGEAR.PULSESOUT must be set more recently than EGEAR.RATIO in order to use exact electronic gearing.

General Information

Type

R/W

Units

Position counts

Range

-32,768 to 32,767

Default Value

1

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1072

No 8 bit Yes

M_01-05-11-000

Related Topics

EGEAR.PULSESIN | EGEAR.RATIO |EGEAR.ON | FB2.SOURCE | FB2.ENCRES | FB2.MODE