EGEAR.PULSESIN
Description
EGEAR.PULSESIN is the number of encoder counts the motor moves for each EGEAR.PULSESOUT number of position counts. EGEAR.PULSESIN must be set more recently than EGEAR.RATIO in order to use exact electronic gearing.
General Information
|
Type |
R/W |
|
Units |
Motor revolutions / Encoder Revolution |
|
Range |
0 to 65,535 |
|
Default Value |
1 |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1070 |
No | 16 bit | No |
M_01-05-11-000 |
Related Topics
MOVE.MOVING | EGEAR.ON | FB2.SOURCE | FB2.ENCRES | FB2.MODE