EGEAR.RATIO

Description

Ratio must be set more recently than EGEAR.PULSESIN or EGEAR.PULSESOUT in order to use EGEAR.RATIO to control electronic gearing.

General Information

Type

TBD

Units

Motor revolutions / Encoder Revolution

Range

-2,000 to 2,000

Default Value

1

Data Type

Float

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1074

No 32 bit No

M_01-05-11-000

Related Topics

EGEAR.ON | EGEAR.PULSESIN | EGEAR.PULSESOUT | FB2.SOURCE | FB2.ENCRES | FB2.MODE