MOVE.RELATIVEDIST

Description

MOVE.RELATIVEDIST specifies the distance the motor moves during a relative move (MOVE.GOREL). Specify MOVE.RELATIVEDIST before initiating MOVE.GOREL.


  • MOVE parameters are only valid when DRV.OPMODE = 2 and DRV.CMDSOURCE = 5.

Example

'This example sets Move.RelativeDist to 655360 (10 motor revolu
'tions, assuming units is 16 bit position units or 65536 
'counts/revolution) and does a relative move.
MOVE.RUNSPEED  = 1000
MOVE.ACC = 10000
MOVE.DEC =  5000
MOVE.RELATIVEDIST = 655360
MOVE.GOREL

General Information

Type

R/W

Units

Depends on UNIT.PROTARY or UNIT.PLINEAR UNIT.ACCLINEAR

Rotary: counts, rad, deg, (Benutzerspezifische Einheiten), 16-bit counts

Linear: counts, mm, µm, (Benutzerspezifische Einheiten), 16-bit counts

Range

N/A

Default Value

N/A

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1134

Yes 64 bit Yes

M_01-05-11-000

Related Topics

MOVE.ACC | MOVE.DEC | MOVE.RUNSPEED