AIN.OVFTHRESH
Description
This parameter defines the over voltage threshold for analog input. If AIN.VALUE is larger than AIN.OVFTHRESH, and AIN.MODE = 3 (user defined fault mode), an over voltage fault is generated.
General Information
|
Type |
NV Parameter |
|
Units |
V |
|
Range |
-10 to 10 |
|
Default Value |
10V |
|
Data Type |
Float |
|
Start Version |
M_01-13-09-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | No |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
|
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|
|
Profinet |
3017 |
DWord | Yes |
| sercos® III | 2 Octets |
| Fieldbus | Instance | Data Size | Data Type |
|---|---|---|---|
| EtherNet/IP | 1018 | 2 Byte Signed | Float |
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
|---|---|---|---|---|
|
Modbus |
2850 |
No | 16 bit | Yes |
Related Topics
Analoger Eingang | AIN.MODE | AIN.UVWTHRESH | AIN.UVFTHRESH | AIN.OVWTHRESH