AIN.UVFTHRESH

Description

This parameter defines the under voltage threshold for analog input. If AIN.VALUE is less than AIN.UVFTHRESH, and AIN.MODE = 3 (user defined fault mode), an under voltage fault is generated.

General Information

Type

NV Parameter

Units

V

Range

-10 to 10

Default Value

-10V

Data Type

Float

Start Version

M_01-13-09-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N No
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Address

Attributes Signed?

Profinet

3015

DWord Yes
sercos® III 2 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 1016 2 Byte Signed Float

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Modbus

2856

No 16 bit Yes

Related Topics

Analoger Eingang | AIN.MODE | AIN.UVWTHRESH | AIN.OVFTHRESH | AIN.OVWTHRESH