EIP.POSUNIT
Description
Position values are scaled according to the Ethernet/IP Position Controller Device standard. One “Position Units” scaling value is defined, which gives the number of actual position feedback counts (at 32 bits per revolution) equal to one position unit.
From WorkBench, this scaling parameter is visible in the Ethernet/IP screen or as EIP.POSUNIT in the terminal. From Ethernet/IP, this value can be accessed at attribute 0x04 Position Units of the Position Controller object.
The default value is 2^16 = 65536, which provides 2^32 / 2^16 = 2^16 counts per revolution. A value of 1 would provide 2^32 / 1 = 2^32 counts per revolution.
General Information
|
Type |
R/W |
|
Units |
N/A |
|
Range |
0 to 4,294,967,295 |
|
Default Value |
65536 |
|
Data Type |
Integer |
|
Start Version |
M_01-05-00-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | No |
| AKD with Position Indexer | No |
| AKD EtherCAT | No |
| AKD CANopen | No |
| AKD BASIC | No |
| AKD SynqNet | No |
| AKD EtherNet/IP | Yes |
| AKD Profinet | No |
| AKD sercos® III | No |
| AKD-N | No |
| AKD-C | No |
Fieldbus Information
| Fieldbus | Instance | Data Size | Data Type |
|---|---|---|---|
| EtherNet/IP | 796 | 4 Byte | Integer |
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1590 |
No | 32-bits | No |
M_01-06-03-000 |
Related Topics