EIP.PROFUNIT

Description

Velocity and Acceleration values are scaled according to the EtherNet/IP Position Controller Device standard. One “Profile Units” scaling value is defined, which affects both velocity and acceleration.

For velocity values, Profile Units gives the number of actual position feedback counts (at 32 bits per revolution) per second equal to one velocity unit. For acceleration values, Profile Units gives the number of actual position feedback counts (at 32 bits per revolution) per second^2 equal to one acceleration unit.

From WorkBench, this scaling parameter is visible in the EtherNet/IP screen or as EIP.PROFUNIT in the terminal. From EtherNet/IP, this value can be accessed at attribute 0x05 Profile Units of the Position Controller object.

The default value is 2^16 = 65536, which provides 2^32 / 2^16 = 2^16 counts per second per revolution. A value of 1 would provide 2^32 / 1 = 2^32 counts per second per revolution.

General Information

Type

R/W

Units

N/A

Range

0 to 4,294,967,295

Default Value

65536

Data Type

Integer

Start Version

M_01-05-00-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT No
AKD CANopen No
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP Yes
AKD Profinet No
AKD sercos® III No
AKD-N No
AKD-C No

Fieldbus Information

Fieldbus Instance Data Size Data Type
EtherNet/IP 797 4 Byte Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1592

No 32-bits No

M_01-06-03-000

Related Topics

EIP.POSUNIT

EtherNet/IP Ansicht "Achse"