MT.CLEAR

Description

MT.CLEAR clears a motion task from the drive. This command needs one argument in order to clear a motion task. A motion task consists of the following parameters: MT.NUM , MT.P, MT.V, MT.CNTL, MT.ACC,MT.DEC, MT.TNUM, MT.MTNEXT , MT.TNEXT

A value of –1 clears all motion tasks in the drive (MT.CLEAR –1).

Example

MT.CLEAR 5: Clear motion task number 5.

After performing a command such as MT.PARAMS 5, the drive displays the following:

5   0.000 Counts   0.000 rpm   0   0.000 rpm/s   0.000 rpm/s   0   0   0 ms

A value of 0 for velocity, acceleration, or deceleration displays motion task as uninitialized.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

MT.NUM , MT.P, MT.V, MT.CNTL, MT.ACC,MT.DEC, MT.TNUM, MT.MTNEXT , MT.TNEXT, MT.SET , MT.LOAD

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Address

Attributes Signed?

Profinet

2265

Word Yes
sercos® III 2 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 266 2 Byte Signed Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

530

No 16 bit Yes

M_01-03-00-000

Related Topics

Fahraufträge