PLS.UNITS

Description

PLS.UNITS is a bit variable which determines the behavior of the eight PLSs available in the drive. This parameter is used to select the units for the PLS pulse.

Examples

Bit Value Behavior

Bit 0 = 0

Position-based PLS handling.

The PLS.STATE parameter displays an active PLS 1 when the position is within the range of PLS.P1 + PLS.WIDTH1

(PLS.P1 <= PL.FB <= PLS.P1+PLS.WIDTH1).

When the parameter PLS.WIDTH1 has been set to the value of 0, this bit will be activated as soon as PLS.FB >= PL.P1.

Bit 0 = 1

Time-based PLS handling.

After PLS.P1 is crossed, the PLS.STATE parameter displays an active PLS 1 for a PLS.T1 ms period of time.

Bit 7 = 0

Position-based PLS handling.

The PLS.STATE parameter displays an active PLS

8 when the position is within the range of PLS.P8 + PLS.WIDTH8

(PLS.P8 <= PL.FB <= PLS.P8+PLS.WIDTH8).

When the parameter PLS.WIDTH8 has been set to the value of 0, this bit will be activated as soon as PLS.FB >= PL.P8.

Bit 7 = 1

Time-based PLS handling.

After PLS.P8 has been crossed. the PLS.STATE parameter displays an active PLS 8 for a PLS.T8 ms period of time.

Continuous position-based PLS handling

PLS.P1 = 720

PLS.WIDTH1 = 360

PLS.UNITS bit 0 (for PLS 1) = low; PLS.T1 is not considered.

PLS.EN bit 0 (for PLS 1) = high

PLS.MODE bit 0 (for PLS 1) = low

 

Time-based PLS handling

PLS.P1 = 720

PLS.T1 = 10

PLS.UNITS bit 0 (for PLS 1) = low; PLS.WIDTH1 is not considered.

PLS.EN bit 0 (for PLS 1) = high

PLS.MODE bit 0 (for PLS 1) = low

General Information

Type

R/W parameter

Units

N/A

Range

0 to 255

Default Value

0

Data Type

Integer

See Also

PLS.EN , PLS.RESET , PLS.STATE , PLS.MODE , PLS.P1 TO PLS.P8 PLS.WIDTH1 TO PLS.WIDTH8 , PLS.T1 TO PLS.T8

Start Version

M_01-02-03-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

34A4h/0

M_01-02-03-000

Fieldbus

Address

Attributes Signed?

Profinet

2337

Byte No
sercos® III 2 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 338 1 Byte Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

674

No 8 bit No

M_01-03-00-000

Related Topics

Programmierbarer Endschalter