CIP Sync User-Defined Data Types
The data types used with AKD2G-SPI drives and CIP Sync have different definitions than those used with the Standard Assembly. The tables below define the data types for CIP Sync.
CIP_Axis
The CIP_Axis data type is the AKD2G CIP Sync Axis Object.
-
- CIP_Axis is not for Studio 5000 Motion Instructions Axis field entries. The Studio 5000 Motion Instructions Axis field entries use the Virtual Axis name of the given axis in the MotionGroup.
The CIP_Axis data type is used in the following:
- CIP_Axis_State_Machine AOI- Axis field entry
- CIP_Drive_Comms AOI-Axis 1 and Axis 2 field entries
- Kollmorgen Supplementary AOIs Axis field entry
- CIP_Axis_Disable
- CIP_Axis_Disable_Streaming
- CIP_Axis_Enable
- CIP_Axis_Enable_Streaming
- CIP_Axis_Fault_Reset
- CIP_Axis_Home
- CIP_Axis_Quick_Stop
-
Size: 64 Bytes
| Name | Data Type | Description |
|---|---|---|
|
Control |
CIP_Control |
Control bits to send to the drive |
|
Status |
CIP_Status |
Status bits received from drive |
|
Input |
CIP_AxisInputData |
Data from the drive |
|
Output |
CIP_AxisOutputData |
Data to the drive |
|
PositionFeedback |
DINT |
Actual Position Value |
|
PositionCommand |
DINT |
Drive’s commanded position |
|
ResponseTimeStamp |
LINT |
Drive’s timestamp of response |
|
RequestedAction |
INT |
State Machine requested action |
CIP_AxisInputData
This data type is a member of the CIP_Axis data type and structure.
-
Size: 12 Bytes
-
Description:
| Name | Data Type | Description |
|---|---|---|
|
Data |
SINT[10] |
|
CIP_AxisOutputData
This data type is a member of the CIP_Axis data type and structure.
-
Size: 16 bytes
-
Description:
| Name | Data Type | Description |
|---|---|---|
|
Data |
SINT[14] |
|
CIP_Control
This data type is a member of the CIP_Axis data type and structure.
-
Size: 4 Bytes
-
Description:
| Name | Data Type | Description | Reference |
|---|---|---|---|
|
Switch_On |
BOOL |
|
CIP Sync Command Assembly Data Structure (105) |
|
Disable_Voltage |
BOOL |
|
|
|
Quick_Stop |
BOOL |
|
|
|
Enable_Operation |
BOOL |
|
|
|
Op_Mode_Specific_4 |
BOOL |
Home Start or Follow Position bit, depending on whether bit 11 (Mode Home) or bit 12 (Mode Cyclic Position) is active. |
|
|
Op_Mode_Specific_5 |
BOOL |
Unused |
|
|
Op_Mode_Specific_6 |
BOOL |
Unused |
|
|
Reset_Fault |
BOOL |
|
|
|
Pause_Halt |
BOOL |
|
|
|
Op_Mode_Specific_9 |
BOOL |
Unused |
|
|
Reserved_10 |
BOOL |
|
|
|
Manu_Specific_11 |
BOOL |
Mode Home bit |
|
|
Manu_Specific_12 |
BOOL |
Mode Cyclic Position bit |
|
|
Manu_Specific_13 |
BOOL |
Unused |
|
|
Manu_Specific_14 |
BOOL |
Unused |
|
|
Manu_Specific_15 |
BOOL |
Unused |
CIP_DynamicMap
CIP_Drive_Comms AOI-DynamicMap field entry
-
Size: 72 Bytes
-
Description:
- Usage: CIP_Drive_Comms AOI-DynamicMap field entry
| Name | Data Type | Description |
|---|---|---|
| Input | CIP_MapInputData | Maps data from the drive |
| Output | CIP_MapOutputData | Maps data to the drive |
CIP_MapInputData
This data type is a member of the CIP_DynamicMap data type.
-
Size: 40 Bytes
-
Description: Map data received from the drive
| Name | Data Type | Description |
|---|---|---|
| Data | SINT[40] | Map data received from the drive |
CIP_MapOutputData
This data type is a member of the CIP_DynamicMap data type.
-
Size: 32 Bytes
-
Description: Map data sent to the drive
| Name | Data Type | Description |
|---|---|---|
| Data | SINT[32] | Map data sent to the drive |
CIP_Status
-
Size: 4 Bytes
-
Description: All connections to the drive Ethernet module are established and data is successfully transferring.
| Name | Data Type | Description | Reference |
|---|---|---|---|
|
Ready_To_Switch_On |
BOOL |
|
See Status Word in CIP Sync Response Assembly Data Structure (106) |
|
Switched_On |
BOOL |
||
|
Operation_Enabled |
BOOL |
||
|
Fault |
BOOL |
||
|
Voltage_Enabled |
BOOL |
||
|
Quick_Stop |
BOOL |
||
|
Switch_On_Disabled |
BOOL |
||
|
Warning |
BOOL |
||
|
STO_Active |
BOOL |
||
|
Remote |
BOOL |
||
|
Target_Reached |
BOOL |
||
|
Internal_Limit_Active |
BOOL |
||
|
Op_Mode_Specific_12 |
BOOL |
Home Attained bit |
|
|
Op_Mode_Specific_13 |
BOOL |
Homing/Cyclic Position Error bit |
|
|
Manu_Specific_14 |
BOOL |
Motion Mode bit (0 for Homing, 1 for Cyclic Position) |
|
|
Manu_Specific_15 |
BOOL |
Following Position bit (for Cyclic Position mode) |