AXIS#.HOME.SET

Description

AXIS#.HOME.SET immediately makes the current position the home position. After using AXIS#.HOME.SET the axis command and feedback will match AXIS#.HOME.P. AXIS#.HOME.SET can be used when the axis enabled or disabled and in torque, velocity or position OpModes (AXIS#.OPMODE). If the axis is in motion when AXIS#.HOME.SET is used, the motion will be stopped and the home position set. Once the home position has been set, the addition move defined by AXIS#.HOME.DIST is not made.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.SET

5008h

01h

Unsigned32

-

-

Write only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6111

1

6111 (0x17df)

AXIS1.HOME.SET

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.SET

6111

Unsigned8

Read/Write

-