EIP.IPADDRESS
Description
This parameter is used to set the IP address of the drive for the EtherNet/IP fieldbus when EIP.IPMODE is set to 0 for static IP.
Examples
Usage
EIP.IPADDRESS is only used when EIP.IPMODE = 0. When setting up the drive with static IP the address must be set using EIP.IPADDRESS and subnet mask must be set using EIP.IPSUBNET. EIP.IPRESET can then be used to apply the specified IP settings.
Code
Set drive to be able to communicate with devices on 192.168.1.x subnet
--> EIP.IPMODE 0 --> EIP.IPADDRESS 192.168.0.1 --> EIP.IPSUBNET 255.255.255.0 --> EIP.IPGATEWAY 192.168.1.1 --> EIP.IPRESET
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-06-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0.0.0.0 to 255.255.255.255 |
|
Default Value |
192.168.0.5 |
|
Data Type |
String |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
EtherNet/IP drives: AKD2G-SPI