EIP.IPRESET
Description
This command is used to acquire a new IP address for EtherNet/IP communication based on which EIP.IPMODE is specified.
Examples
Usage
After making changes to EtherNet/IP IP parameters, EIP.IPRESET can be used to acquire a new IP address. When the command is issued, the drive will reset the network stack on the EtherNet/IP ports, disconnecting any devices that may be connected via those ports. EIP.IPADDRESS and EIP.IPSUBNET cannot be set to 0.0.0.0 or the command will return an error.
Code
Set drive to use static IP of 192.168.0.1
--> EIP.IPMODE 1 --> EIP.IPADDRESS 192.168.0.1 --> EIP.IPSUBNET 255.255.255.0 --> EIP.IPRESET
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-00-001 |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |
Variants Supported
EtherNet/IP drives: AKD2G-SPI