EIP.IPGATEWAY
Description
This parameter is used to set the gateway IP of the drive for the EtherNet/IP fieldbus when EIP.IPMODE is set to 0 for static IP. It determines the IP addresses the drive can communicate with outside of its current subnet.
Examples
Usage
EIP.IPGATEWAY is only used when EIP.IPMODE = 0. If communication with devices outside of the drive's subnet is desired, then the gateway IP should be set based on the IP address of devices outside of the subnet. The EIP.IPRESET command can then be used to apply the specified IP settings.
Code
Set drive to be able to communicate with devices on 192.168.1.x subnet.
--> EIP.IPMODE 0 --> EIP.IPADDRESS 192.168.0.1 --> EIP.IPSUBNET 255.255.255.0 --> EIP.IPGATEWAY 192.168.1.1 --> EIP.IPRESET
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-06-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0.0.0.0 to 255.255.255.255 |
|
Default Value |
0.0.0.0 |
|
Data Type |
String |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
EtherNet/IP drives: AKD2G-SPI