MC_EStop

PLCopen motion icon

 Function - Causes an emergency stop (E-stop).

  • See Function Blocks - General Rules about how inputs and outputs work.
  • Call MC_EStop to generate an emergency stop for an axis.
  • Call MC_ResetError to reset the emergency stop.
  • Actions of an E-stop:
    • Stops motion interpolation.
    • Clears all moves from the queue (active and next).
    • Changes the axis state to ErrorStop.
    • Request the drive to open the position loop and disable the drive.
  • The E-stop remains in effect until the application calls MC_ResetError to reset the E-stop.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

En

BOOL

FALSE, TRUE

N/A

No default

A positive transition of this input causes an E-stop on the specified axis.

Axis

AXIS_REF

1 to 256

N/A

No default

The AXIS_NUM element of the AXIS_REF structure.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

  • Indicates the E-stop was executed.
  • If an invalid Axis input was specified, this output is not energized and no E-stop is performed.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

(* MC_EStop ST example *)
ON EStopButton DO
MC_EStop( Axis1 );
MC_EStop( Axis2 );
END_DO;

See Also

MC_ResetError