MC_MoveAdditive
Function Block - Performs a single-axis move for a specified distance from the endpoint of the previous move.
- See Function Blocks - General Rules about how inputs and outputs work.
- It is typically used with Abort specified at the BufferMode input.
- If BufferMode is not Abort, this move is identical to an MC_MoveRelative.
-
-
- This function block starts a motion-related action and stores data for calculations and error checking.
- If using a dual-core controller, see Program a Multi-Core Controller.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, request to queue the move. |
|
Axis |
AXIS_REF |
1 to 256 |
N/A |
No default |
Name of a declared instance of the AXIS_REF library function.
|
|
Distance |
LREAL |
No range |
User units |
No default |
Distance to add to the endpoint of the previous move. |
|
Velocity |
LREAL |
No range |
User units / sec |
No default |
Velocity setpoint. |
|
Acceleration |
LREAL |
No range |
User units / sec2 |
No default |
|
|
Deceleration |
LREAL |
No range |
User units / sec2 |
No default |
|
|
Jerk |
LREAL |
No range |
User units / sec3 |
No default |
|
|
BufferMode |
SINT |
Enumerated |
N/A |
No default |
The specified buffer mode.
|
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
Indicates the move completed successfully. |
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
High from the moment the Execute input goes high until the time the move is ended. |
|
Active |
BOOL |
FALSE, TRUE |
N/A |
Indicates this move is the Active move. |
|
CommandAborted |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command was aborted by another function block. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
Indicates either:
|
|
ErrorID |
INT |
No range |
N/A |
|
Time Diagram
These images show two examples of the combination of two Function Blocks (FBs) while the axis is in Discrete Motion state:
- The left part of the diagram illustrates when the second FB is called after the first one.
- If the first reaches the commanded distance 6000, and the velocity is 0 (zero), the output Done causes the second FB to move to the distance 10000.
- The right part of the diagram illustrates when the second move FB starts the execution while the first FB is still executing.
- The first motion is interrupted and aborted by the Test signal during the constant velocity of the first FB.
- The second FB:
- Adds on the previous commanded position of 6000 the distance 4000.
- Moves the axis to the resulting position of 10000.
Figure 1: Time Diagrams: First and Second FBs
Figure 2: Time Diagram
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MC_MoveAdditive ST example *)
Inst_MC_MoveAdditive( MovAddReq, Axis1, 123.456, 100.0, 100.0, 100.0, 0, 0 );
//Inst_MC_MoveAdditive is an instance of MC_MoveAdditive function block
MovAddDone := Inst_MC_MoveAdditive.Done;
//store Done output into user defined variable
See Also