MLAxisGenPos

Pipe Network motion icon

 Function - Returns the generator position of the axis.

  • Returns TRUE if the internal generator axis is ready.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Position

LREAL

No range

User units

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Generator_Position := MLAxisGenPos(PipeNetwork.Axis1 ) ;

See Also