MLAxisPipePos
Function - Returns the pipe position of the axis.
-
-
- This function or function block returns cached data.
- See Program a Multi-Core Controller.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
1 to 1024 |
N/A |
No default |
ID of the Axis block. |
|
Speed |
LREAL |
No range |
User units / sec |
No default |
|
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
FALSE, TRUE |
N/A |
|
|
Position |
LREAL |
No range |
User units |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Axis1_Pipe_Position := MLAxisPipePos (PipeNetwork.Axis1 ) ;
See Also