RecipeOpen
This function/function block was added in KAS 5.00.
Function Block - Open a recipe file and create a recipe object.
Recipe files opened with RecipeOpen must include a recipe definition section.
- Instance sections are optional.
- Recipes without instance sections can be opened and used later with RecipeStoreInstance to create instances from active program data.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, load a recipe file. |
||||||
|
RecipeFile |
STRING |
No range |
N/A |
No default |
The location of the recipe file. |
||||||
|
RecipeFormat |
SINT |
Enumerated |
N/A |
No default |
|
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the function block is executing. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
DINT |
Enumerated |
N/A |
|
|
RecipeID |
UDINT |
No range |
N/A |
The ID of the recipe object. |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_RecipeOpen(True, 'Parts.xml', RCP_FMT_XML); IF Inst_RecipeOpen.Error THEN errorMessage := MC_ErrorDescription(Inst_RecipeOpen.ErrorID); ELSE recipeID = Inst_RecipeOpen.RecipeID END_IF;
// Inst_RecipeOpen(True, '/usbflash/recipes/Parts.xml', RCP_FMT_XML); IF Inst_RecipeOpen.Error THEN errorMessage := MC_ErrorDescription(Inst_RecipeOpen.ErrorID); ELSE recipeID = Inst_RecipeOpen.RecipeID END_IF;
See Also