RecipeStoreInstance

This function/function block was added in KAS 5.00.

PLCopen motion icon Pipe Network motion icon

 Function Block - Store the present values of the program data in a recipe instance.

  • If an instance with the specified name already exists, the values in that instance are overwritten.
  • If no instance exists with the specified name, a new instance with the specified name is created.
  • No range validation is performed while storing.
    • Validation is deferred until a later call to RecipeApplyInstance.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

Execute

BOOL

FALSE, TRUE

N/A

No default

On the rising edge, save the program data into the named recipe instance.

RecipeID

UDINT

No range

N/A

No default

  • The ID of the recipe object to use.
  • RecipeID is the handle ID returned by the RecipeOpen function block.

Name

STRING

No range

N/A

No default

  • The name of the new instance.
  • If Name is an empty string, the instance is assigned the name 'Instance'.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Done

BOOL

FALSE, TRUE

N/A

If TRUE, the command completed successfully.

Busy

BOOL

FALSE, TRUE

N/A

If TRUE, the function block is executing.

Error

BOOL

FALSE, TRUE

N/A

If TRUE, an error has occurred.

ErrorID

DINT

Enumerated

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Inst_RecipeStoreInstance(True, recipeID, 'Cogs'); 
IF Inst_RecipeStoreInstance.Error THEN    errorMessage := MC_ErrorDescription(Inst_RecipeStoreInstance.ErrorID); END_IF;

See Also