RecipeQuickLoad
This function/function block was added in KAS 5.00.
Function Block - Load a recipe file and immediately apply the items it contains.
RecipeQuickLoad loads a recipe instance without requiring that a recipe definition be loaded first.
- Only the first recipe instance found in the file is applied.
- When ContinueOnError is TRUE, all validation errors encountered are added to the controller log.
- See Log Messages tabs.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, request loading and applying the recipe stored in the file RecipeFile. |
||||||
|
ContinueOnError |
BOOL |
FALSE, TRUE |
N/A |
No default |
|
||||||
|
RecipeFile |
STRING |
No range |
N/A |
No default |
The location of the recipe file. |
||||||
|
RecipeFormat |
SINT |
Enumerated |
N/A |
No default |
|
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the function block is executing. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
DINT |
Enumerated |
N/A |
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_RecipeQuickLoad(True, False, 'CogsRecipeInst.xml', RCP_FMT_XML); IF Inst_RecipeQuickLoad.Error THEN errorMessage := MC_ErrorDescription(Inst_RecipeQuickLoad.ErrorID); END_IF;
See Also