AXIS#.HWEN.MODE

Description

Selects whether AXIS#.CLRFAULTS is performed on the rising edge of the hardware enable input

Examples

Usage

0 (default): perform AXIS#.CLRFAULTS on the rising edge of the hardware enable input

1: do not perform clear faults on the rising edge of the hardware enable input

Code

--> AXIS1.HWEN.MODE 0
--> AXIS2.HWEN.MODE 1

Context

For more information on hardware enable, refer to Enable/Disable.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also AXIS#.HWEN.SOURCE, AXIS#.HWEN.STATE, AXIS#.CLRFAULTS

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HWEN.MODE

5009h

02h

Unsigned8

-

-

Read/Write

No

AXIS2.HWEN.MODE

5109h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

7000

1

7000 (0x1b58)

AXIS1.HWEN.MODE

Unsigned8

Read/Write

Yes

72536

2

7000 (0x1b58)

AXIS2.HWEN.MODE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HWEN.MODE

7000

Unsigned8

Read/Write

-