AXIS#.MOTOR.ICONT

Description

This parameter is the motor continuous current.


  • This parameter is required to be configured for all motor types.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

0.1 to 500

Default Value

1

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.ICONT

500bh

10h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MOTOR.ICONT

510bh

10h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6204

1

6204 (0x183c)

AXIS1.MOTOR.ICONT

Unsigned32

Read Only

Yes

71740

2

6204 (0x183c)

AXIS2.MOTOR.ICONT

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.ICONT

6204

Float

Read Only

-