FB#.HALLMAP.U

Description

FB#.HALLMAP.U reads and writes to a mapping register used to correct mis-wired motors without physically changing the wiring. This keyword only effects feedback devices that have halls (see FB#.SELECT for feedback types with halls).

FB#. HALLMAP.U can be set to one of the following values:

Value

Description

0

The output is the U input value. (Default)

1

The output is the V input value. (Swap U with V)

2

The output is the W input value. (Swap U with W)

3

The output is fixed at 0.

4

The output is U input inverted value. (When input U=0, U output is 1)

5

The output is V input inverted value. (When input V=0, U output is 1)

6

The output is W input inverted value. (When input W=0, U output is 1)

7

The output is fixed at 1.

Versions

Action Version Notes
Implemented 02-10-00-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 7

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.HALLMAP.U

3500h

1bh

Unsigned8

-

-

Read/Write

No

FB2.HALLMAP.U

3501h

1bh

Unsigned8

-

-

Read/Write

No

FB3.HALLMAP.U

3502h

1bh

Unsigned8

-

-

Read/Write

No

FB4.HALLMAP.U

3503h

1bh

Unsigned8

-

-

Read/Write

No

FB5.HALLMAP.U

3504h

1bh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30740

1

30740 (0x7814)

FB1.HALLMAP.U

Unsigned8

Read/Write

Yes

30741

1

30741 (0x7815)

FB2.HALLMAP.U

Unsigned8

Read/Write

Yes

30742

1

30742 (0x7816)

FB3.HALLMAP.U

Unsigned8

Read/Write

Yes

30743

1

30743 (0x7817)

FB4.HALLMAP.U

Unsigned8

Read/Write

Yes

30744

1

30744 (0x7818)

FB5.HALLMAP.U

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.HALLMAP.U

30740

Unsigned8

Read/Write

-

FB2.HALLMAP.U

30741

Unsigned8

Read/Write

-

FB3.HALLMAP.U

30742

Unsigned8

Read/Write

-

FB4.HALLMAP.U

30743

Unsigned8

Read/Write

-

FB5.HALLMAP.U

30744

Unsigned8

Read/Write

-

Related Topics

FB#.HALLSTATE

FB#.HALLMAP.V

FB#.HALLMAP.W

FB#.SELECT