FB#.SCALED.P

Description

FB#.SCALED.P is the scaled feedback position. See Scaled Feedback for details on the calculation.

Versions

Action Version Notes
Implemented 02-07-01-000

General Information

Type

Read Only

Units

Depends on FB#.SCALED.PIN

and FB#.SCALED.POUT

Range

Full position range

Default Value

N/A

Data Type

Float

See Also

FB#.P

Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Related Topics

Scaled Feedback