FB#.SCALED.PIN

Description

FB#.SCALED.PIN is the numerator of the FB#.SCALED.P scaling ratio.

Versions

Action Version Notes
Implemented 02-07-01-000

General Information

Type

Read/Write

Units

N/A

Range

1 to 4,294,967,295

Default Value

360

Data Type

Integer

See Also

FB#.SCALED.P

Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Related Topics

Scaled Feedback