FB#.SCALED.ZERO

Description

This command updates FB#.SCALED.P to 0 by changing FB#.SCALED.OFFSET to the negative value of FB#.SCALED.P before it is zeroed.

Example

Code

-->FB1.SCALED.OFFSET
1999.999 [deg]
-->FB1.SCALED.P
417447.831 [deg]
-->FB1.SCALED.ZERO
-->FB1.SCALED.OFFSET
-415447.804 [deg]
-->FB1.SCALED.P
0.000 [deg]

Versions

Action Version Notes
Implemented 02-10-02-000

General Information

Type

ReadOnly

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

FB#.SCALED.P

FB#.SCALED.OFFSET

Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Related Topics

Scaled Feedback