WS.DISARM

Description

This command disables wake and shake immediately. Feedback type is not relevant for this command. If WS.ARM has been issued, the request to execute the wake and shake algorithm at the next enable is cancelled. WS.STATE is set to IDLE.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

N/A

Start Version

M_01-04-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No

 

*For PROFINET, write a value of 0 into the PNU to execute a command.

Related Topics

Wake and Shake Overview