Motion Bus and Fieldbuses

Depending on the fieldbus used in your project (i.e., EtherCAT, PROFINET, etc.), you must use the configuration tools.

The controller can be connected to multiple Ethernet devices simultaneously by connecting a switch to the top of the controller:

AKD PDMM and PCMM

PCMM2G

X32 port on the top of the controller:

Figure 1: AKD PDMM and PCMM X32 switch connections.

X31 or X32 port on the top of the controller:

Figure 2: PCMM2G X31 and X32 switch connections.

EtherCAT

EtherNet/IP

The KAS Runtime includes a fully integrated EtherNet/IP Adapter driver and Scanner driver for exchanging data with EtherNet/IP tag-based devices such as PLCs.

Modbus and TCP/IP

PROFINET

This fieldbus is PROFIBUS over Ethernet.

We define one controller and have one or more devices.

Configuration

OPC UA

The Open Platform Communications Unified Architecture (OPC UA) is a standardized, platform-independent communication protocol developed by the OPC Foundation.

  • It is designed for secure, reliable, and interoperable machine-to-machine communication in industrial automation environments.
  • The KAS Runtime includes a fully integrated OPC UA Server driver for exchanging data with OPC UA client devices (e.g., PLC, HMI, etc.)
  • See OPC UA Server.