You are here: Technical References > Motion Library > Motion/Pipe Network > MLAxisGenReadSpd

FunctionMLAxisGenReadSpdPipe Network motion icon

Description

Get the speed of the internal generator of an axis.

Arguments

Input

AxisID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

Output

OK

Description

 

 

Data type

BOOL

 

Unit

n/a

Speed

Description

Returns Axis Speed value

 

Data type

LREAL

 

Unit

User unit/sec

Related Functions

MLAxisGenReadDec

MLAxisGenReadAcc

Example

Structured Text

 

Axis1_Speed := MLAxisGenReadSpd( PipeNetwork.Axis1 ) ;

 

Ladder Diagram

MLAxisGenReadSpd: LD example

 

Function Block Diagram

MLAxisGenReadSpd: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™