The SD card is used for backing up and restoring the data from a PDMM or PCMM.
Backing up may be performed in either of two ways.
For a complete backup of both the controller and drive, use the Web Server backup.
Restoring information to the controller may be performed in either of two ways. Both methods restore the controller (and PDMM drive) with whatever was saved to the SD card.
The 7-segment display will show the chasing lights animation while the backup or restore is occurring. Warning! Do not modify the files on the SD card as this could result in the Restore function failing.
If you have multiple PDMM or PCMM backup configurations, you will need to use one SD card per backup configuration.
|
Copyright © 2015 Kollmorgen™ |
|