You are here: Using the PDMM or PCMM Controller > Using the Web Server > Using the KAS Web Server > WebServer Backup and Restore

Backup & Restore from the Web Server

These functions are used to replicate a PDMM or PCMM (Backup and then Restore) to or from the SD card. The elements that are backed up or restored are the firmware, the network configuration, the Retain Variables, and the PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events application.

The PDMM and PCMM are available with different CPU speed variants (800 MHz and 1.2 GHz). The PDMM and PCMM models have the same functionality, but due to the CPU speed differences an application designed for the 1.2 GHz model may not execute as expected on the 800 MHz model. The Restore will not allow a higher speed model to be replaced with a lower speed model. The Restore will allow a lower speed model to be replaced with a higher speed model, if the Backup contains the model specific RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running firmware file.

  800 MHz Restore 1.2 GHz Restore
800 MHz Backup Yes Yes - If 1.2 GHz Runtime file is included in the Backup
1.2 GHz Backup No Yes

 

Webserver Backup Tab

Webserver Restore Tab

Webserver Import Export Tab


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™