The PDMM is equipped with ample memory to handle the most challenging programs.
| Memory Type | Amount | Purpose |
|---|---|---|
| Flash | 64 MB | Non-volatileinformation is stored in a specific memory to remain accessible even when the application has been powered off memory |
| SD Card slot | 2+ GB | Backup and Restore functionality as well as moving data. See SD Card Support for more information. |
| DDR RAM | 256 MB | everything else |
|
Copyright © 2015 Kollmorgen™ |
|