You are here: Technical References > Application Modules > Integrating Non-Standard I/O Devices Into a KAS EtherCAT Network with an AKC Controller > Example

Example

The rest of this application note explains, in detail, the process of creating and utilizing an external EtherCAT Configuration file for a AKC system with standard and non-standard components. The EtherCAT network in this example consists of the following.

 

1 - KAS IDE – Scan Standard Components with IDE Scan

2 - EtherCAT Configurator – Add base XML file and Startup the Ethercat Configurator

3 - EtherCAT Configurator – Nodes Setting

4 - EtherCAT Configurator – Cycle time setting

5 - EtherCAT Configurator – Distributed Clock Setting

6 - EtherCAT Configurator – Export the XML file

7 - KAS IDE – Import the ENI file

8 - KAS IDE – Adjust EtherCAT Address

9 - KAS IDE – Initial Settings

10 - KAS IDE – Reading and Writing AKD I/O

11 - KAS IDE – Reading and Writing Parameters for Non-Standard I/O

12 - KAS IDE – Read and Write Parameters for Remote I/O

13 - Reference: EtherCAT Configurator Image file


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™